Other Parts Discussed in Thread: TIDA-01638
Good day Colleagues,
Could you help the customer with the TPS2121 for the Automatic Switchover Between Two 5-V Supplies?
IN1 - is a primary +5V input. IN2 - secondary +5V input. Both inputs can be connected simultaneously.
The TPS2121 should use the primary (IN1 +5V) input to the output even if the secondary (IN2 +5V) is connected. And switch to the IN2 if IN1 was disconnected.
the task is similar to what the datasheet on page 27 (pic 10-12) and the TIDA-01638 (
https://www.ti.com/tool/TIDA-01638) design used for but for +5V in customer's case.
Could you help to find an optimum resistors values for pins PR1, ST, OV1 and OV2? What ref voltage customer should use for the SP2 pin?
Thank you, Mikhail