Other Parts Discussed in Thread: CSD25402Q3A
Hi,
Please tell me about the drive capability of /BATDRV pin and the compatibility with the FET under consideration.
The input voltage is 19V, the system voltage is 16.8V, and the battery in use is 4 cell Li-ion.
Customers are considering the following FETs.
・TPCA8120
・RS1E260ATTB
1.
The data sheet has the following description.
However, it cannot be determined whether the above FET can be driven.
Is it possible to drive the above FET?
2.
If /BATDRV performs maximum output operation, is there a possibility that BA25703A will operate unstable?
What happens to the BQ25703A if the Pch gate cannot be set to High completely?
Could you give me your advice?
Best regards,
Yusuke