This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3404HV: Fluctuation of output current

Part Number: LM3404HV
Other Parts Discussed in Thread: LM3404

Hi support team,
Please let us know about the specification and operation of the LM3404HVMR.

I am prototyping based on "Design Example 1" of the data sheet.

If the input voltage (24V) is fluctuated in 1V increments in the range of 18V to 36V, the output current will fluctuate by several mA.

   18V: 132.2mA (actual measurement value)
   36V: 140.2mA (actual measurement value)

Is this current fluctuation within the standard range of the product?
Or is there anything that can be inferred as a factor that causes the output current to fluctuate?
A prototype circuit is attached, so please let us know if you notice anything.

Regards,
Dice-K