hi Sir
i want to use the TPS56637 for a negative ouput
spec
vin:24v/
vout:-5v/5A
Does it suit for negative outpur?
Or any suggestion?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Sir
i want to use the TPS56637 for a negative ouput
spec
vin:24v/
vout:-5v/5A
Does it suit for negative outpur?
Or any suggestion?
Hi Alex,
TPS56637 can get negative output. But for this application, the input voltage across the device is Vin to Vout. Thus, the input voltage range is Vin_min to Vin_max-Vout, where Vout is a positive value.
So if you want to get -5Vout, the max Vin should be under 28V-5V=23V. Can't support 24V.
The attached link is for reference.
https://www.ti.com/lit/an/slva933/slva933.pdf
Thanks,
Lishuang