This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Team
Our customer is considering using the voltage output from the Vcc pin to control the EN pin on the TPS56C230.
(A 100kΩ resistor is connected between VCC and EN)
However, if you check Figure.17 of the data sheet, the voltage of VCC rises after EN rises.
Therefore, I think that the EN pin cannot be controlled by the output voltage of the VCC pin.
Is this perception correct?
Best Regards,
Y.Ottey
Hi Ottey,
Yes. Vcc is the output of an internal LDO and ramps up after both Vin and EN higher than their respective threshold. So the EN pin cannot be controlled by the output voltage of the VCC pin.
Thanks,
Lishuang