Other Parts Discussed in Thread: LM2662
Hi Expert,
Customer is considering about LM2660 absolute max.
Power dissipation VSSOP (DGK) : max 500mW
Operating junction temperature : max 85C
> It is described in the Absolute Maximum Ratings section, but is this the operating temperature range?
And, Rja=250C/W (JEDEC board)
Also datasheet describe as below,
(3) The maximum allowable power dissipation is calculated by using PDMax = (TJMax − TA)/RθJA, where TJMax is the maximum junction temperature, TA is the ambient temperature, and RθJA is the junction-to-ambient thermal resistance of the specified package.
In case of TA=25C, Rja=250C/W, Pdmax=500mW, Tjmax will be 150C. (I know, Rja is depend on each board condition. And, it is depend on Ta max.)
I think, Tjmax value for Absolute Maximum Ratings is 150C, is it correct?
or
Tjmax value for Absolute Maximum Ratings is 85C, and, Rdmax is 500mW. It is calculated with low Ta and low Rja conditions. ?
Thanks
Muk