Other Parts Discussed in Thread: TL1431, , TL431
Question about using the TL1431 as a delay circuit in the comparator mode. This would be open loop mode with a resistor to the ref pin and capacitor to ground. The ref input through the resistor and the cathode (through resistor) are supplied from the same power supply (28V), but the reference voltage lags due to the RC time constant when the 28v starts up. When the 28V supply ramps up, the voltage on the reference pin will ramp up much slower and when the reference crosses the threshold, the cathode will go "low" switching a PNP transistor. The circuit is similar to one shown in the SLV987A app note. The data sheet shows Ii(ref) (-55C to 125C) to be 5uA max, so the resistor value in the RC network on the reference input is selected to provide >> 5 uA. By the time the voltage on the ref input gets to about 2.5V, the 28V is fully up and the cathode resistor was selected to provide the recommended Ika of at least 1mA. I have not seen a specific application for a xx431 as delay circuit so would like to know if there are any issues to be aware of. In the app note SLVA987A, it states that Vka(low) can vary per device and depends on Vref, Ika, and Iref. Is there a safe maximum value for Vka(low) that can be used for design purposes? Figures 3 and 4 on the TL1431 data sheet show Ika vs Vka, with Vka max at about 2.5V (at 25C).