This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87524-Q1: the output voltage before I2C configure?

Part Number: LP87524-Q1
Other Parts Discussed in Thread: AWR2243, , TIDEP-01012

Hello team

    I plan to choose LP87524 to supply AWR2243(1.0V/1.8V/1.2V/3.3V), because I need to use MCU to configure the register of LP87524 through I2C interface before supply 2243. it will take 5ms(include MCU boot), i want to know the default output before configure? 2. I2C device address of all LP87524 is 0x60? that means I don't connect I2C together if I use several pcs LP87524, is it right?

    thanks!