Hi
I have been looking to bq24064 Battery Linear charger ic for my new design.
I have doubt in IC specs like
The maximum recommended Input voltage of IC is 16.5V
but Overvoltage protection of the IC is 11.7 maximum. Can i able to charge the IC with 12V to 14V input.
If I do so Overvoltage protection will be enabled ?
Please clarify me the difference between Input over voltage protection and recommended input voltage.
bq24064 EVM board also says that IC will be disabled if Vin is greater than Vovp,
Clarify me in this.
Thanks