Other Parts Discussed in Thread: LMZM33604
Hi!
We would like to use LMZM33606 as main DC-DC buck converter.
Our design requires 4 independent power rails : 12V (3A), 5V (5A), 3.3V (5A), 3.3V (5A).
We are planing to use 4x LMZM33606 (or 1x LMZM33604 and 3x LMZM33606) sharing same power input connector.
Input power source will be 6S battery 25V (8S is also should be supported 34V).
I would like to clarify couple of questions:
1) Do we need to use same input capacitors to each LMZM33606 module ? 2x10uF ceramic + 33uF tantalum per LMZM device ?
Is it possible to combine it or to use less count of capacitors ?
DS " 7.3.2 Input Capacitor Selection
The LMZM33606 requires a minimum of 20 μF of ceramic type input capacitance. Use only high-quality ceramic
type X5R or X7R capacitors with sufficient voltage rating. TI recommends an additional 33 μF of non-ceramic
capacitance for applications with transient load requirements."
2) What do you recommend against of inrush current when there will be many ceramic caps at high side of the device ?
Is there any good practice or "rule of thumb" schematics from TI ?
We would like to avoid overvoltage case described in "AN88".
Many thanks!