This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24130: Charge termination

Part Number: BQ24130
Other Parts Discussed in Thread: BQ24133

The BQ24130 is in some places referred to as host controlled and in some places as stand-alone.  slvt145r.pdf states it as stand-alone, but the datasheet states hosted, while an older SLYT420 states it as both. My question is: Will the BQ24130 stop charging when the charging current reaches a certain minimum level?

If no, how can the charger be seen as 'stand-alone'?

If yes, how is the level set, or what is the level? Are there eny special setup / connections needed to make the charger act in stand-alone mode?

Thank you for your support!

Best regards

Jens Christian

  • Jens,

    BQ24130 is a standalone device. I agree, the host controlled label is very confusing. The BQ24130 can have its fast charge and precharge current settings changed on-the-fly using the DAC or GPIOs on an MCU. Alternatively, these values can be fixed with resistors and the device will operate truly as a standalone device.

    I hope this clarifies this.

    Best Regards,

    Ricardo 

  • Thank you Ricardo,

    One thing is still outstanding for me - how does the BQ24130 stop charging - will it stop charging at some point, or continue, unless an external MCU does "something"?

    Best regards

    Jens Christian

  • Jens,

    I see your concern now. This device is a bit difference and I understand why it is labelled as host controlled. 

    It is the responsibility of the host controller to driver ISET1 low when charging is complete. This can be done with an MCU or external logic.

    If you are interested in a truly standalone solution, consider the BQ24133.

    Best Regards,

    Ricardo