Hi, I am going to use TPS56637 for my system.
I have two questions using TPS56637.
--------------------
Question 1.
To enable TPS56637, in the datasheet
"Driving EN high or leaving this pin floating enables the converter."
I want to make auto enable TPS56637 when Vin ramps up.
Which way would you recommend for this? Are both way have same internal soft start time? (Tss for 2ms?)
1. Using two resistors for voltage divide from VIN to make EN high.
2. or Just floating?
-------------------------------------
Question 2.
TPS56637's absolute maximum of VIN voltage is 32V.
and operating max VIN voltage is 28V.
-----------------------------------------------------------------------------
I am going to use 7s Li-Ion battery for this system. This will make max VIN voltage 29.4V.
Because there is Over voltage protection in Battery, so the battery will never go up above 29.4V.
In this case, can I use TPS56637 for this system? (About 1.4V will over when I use TPS56637 in my system )
Thanks.