Other Parts Discussed in Thread: TPS92612-Q1
Hi, team.
Is it possible to use the TPS92638 by sharing the current of 5mA each?
I want to switch to 5mA / 10mA / 15mA as shown in the figure.
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, team.
Is it possible to use the TPS92638 by sharing the current of 5mA each?
I want to switch to 5mA / 10mA / 15mA as shown in the figure.
Best Regards,
Hi, i think it can work but the precise is about 20%.
For higher accuracy, you can choose 3 pcs of TPS92611 in this case.
Is it possible to use 3 pcs of TPS92612-Q1?
TPS92612-Q1 is smaller and cheaper.
Best Regards,
TPS92612-Q1 can also work but there is no diagnostic function. So if there is no need for fault detection and report, i think 612 also works.