Other Parts Discussed in Thread: TPS92611-Q1
Hi,
Customers will have TPS92610-Q1 / TPS92611-Q1.
* Questions
The design specification is the output current Type 260mA1CH, Type450mA1CH.
For the 260mA specification, it is assumed to be available as one TPS92610-Q1.
However, two or more 450mA specifications may need to be used in parallel use.
In relation to this, please check if there is a possibility of parallel use for the corresponding two types of ICs and if there is a possibility of parallel use for PWM and Fault Signal as well.
Also, if there are any related documents (applications, calculators, etc.) available in parallel, please share them with us.