Hello,
I am using BQ24170 in my application for charging 3S Li-ion 12V battery. I am facing an issue of very high inrush current on the Battery +Ve. Attached is the schematic of the Charging section and the power supply sections. Please not, there is no Charging adaptor connected in this scenario.
I am in the process of doing the root cause analysis of the source of this peak current and need help for the same. I suspect it is either because of the capacitors or the mosfet Q14. I tried below experiments:
Experiment 1:Measurement of the peak current.
1. Since I do not have a current probe, to measure the peak current I replaced the fuse F1 with 0.5E resistor and tried to measure the drop across it while plugging the battery.
2. Attached is the waveform. The peak drop is ~6V which means the current peak is ~12A which is very high.
Experiment 2: Measurement of the battery mosfet Q14 gate turn on time
1. The gate turn on time measured is ~194us which is ~5Khz.
2. One observation I had is if I remove the R296 which is series resistor with the gate of the PMOS, I still see Vsys node same as Vbat node when battery is plugged. I did not understood this. If the gate is floating, it can still conduct?
Experiment 3: Decrease the capacitance of the Vbat and Vsys lines by removing C273 and C254.
With this experiment there is no change in the peak current.
Can you please look at the schematics and waveforms and help with some pointers to this? 4174.Power Supply.pdf3750.waveforms.docx