Hi,
I would like to ask you about how to use the TPS65261 device.
(question 1)
If I only use two Buck converters, should I just set ENx to L for an unused Buck converter?
Or do I need other settings?
(Question 2)
Is it possible to connect two Buck converters to increase the output current?
If possible, can I connect with any Buck converter?
For example, connecting Buck1 and Buck2.
Best regards,