Other Parts Discussed in Thread: GAUGEPARCAL
The documentation is very lacking regarding which voltage parameters need to be set per CELL and which are set per STACK. You cannot use the default values (as one suggested) because those were set up for a single cell.
1. Can you please provide documentation on which voltage parameters should be set to STACK voltage? For example, EMF, EDVC0, EDVC1, EDVR1, EDVR0, EDVT0, EDVTC, next the fixed EDV0, EDV1, EDV2, and finally the Voltage 0% DOD, 10% DOD, etc.
2. Is there any example of walking through the values for a given multi-cell battery? This would be IMMENSELY helpful to all of us. Just pick any multi-cell battery and explain specifically how to configure the gauge based on the output of GAUGEPARCAL (OCV11.txt, GPC_CEDV.txt, etc.)