Other Parts Discussed in Thread: TPS548B28,
Hello,
I prepare calculations according to paramiters of my project. To check that my Exel formulas are correct I repeated calculations from datasheet and found some violations.
1. For example
- chapter 8.2.2.3, equation (11), my result is 3.3A (in datasheet 4.12A)
- chapter 8.2.2.4, equation (14), my result is 16.33A (in datasheet 13.88A). Seems like you didn't multiply result to (1/0,85)
Could you please check this calculations?
2. Please clarify, in equation (15), (16) and (17) I have to use I_lim_valley. Why in (15), (16) and (17) is used 15A, not value from (14) (variable also named I_lim_value)?
Also relations between equations (4) and (15) make confusion. I suppose I need to use (14)
Thank you