This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have had a repetitive problem similar as posted here https://e2e.ti.com/support/power-management/f/196/t/706932?tisearch=e2e-sitesearch&keymatch=LT1054
In my design, we convert from a 15VDC power bus generated from a DC/DC converter to -15VDC with the LT1054. The load are several op-amps and other integrated circuits which have dual supply (15VDC and -15VDC), but the -15V total consumption is not greater than 34mA when we are working in normal operation. The majority of the circuit is conformed by the OPA192 model, and we have not any microcontroller nor digital circuit.
The principal problem with the LT1054 is that we had to debug so many PCBs because it fails at startup, supplying a Vout=0.6-0.7V. The architecture which we used is shown below.
(All the capacitors are SMD ceramic models)
In order to fix it, we have had to replace the LT1054, or in the worst cases, disconnect or replace some op-amps from the load. We have so many suspections about this:
-We could have an startup current from the load which could cause the fail. In order to fix it, we tried the architecture using the FB/SHDN pin, but we are not sure if is correct and what are the limitations to it, because it doesn't work always. We have tested changing the capacitor value in order to start the LT1054 later, but it doesn't work.
-Any of the op-amps from the load is forcing a positive voltage in the N15VDC somehow, which as said in the datasheet, is not recomendable. In one hand, there are a bunch of PCBs which are working with this design, so we doubt that this could be the real problem because we think it doesn't depends on the component tolerances, but in the other hand, the actual implementation doesn't allow us to implement the transistor solution showed in the datasheet, so we couldn't check that...
-There are some issues with the DC/DC converters (noise or disturbances) which affects the LT1054. Our 15VDC converter is implemented as shown below:
But in the P28VDC line there are others DCDC converters in order to supply other parts of the circuit. In our debugging adventure, we have tested that disconnecting some of them affects positively to the LT1054, but unfortunately, they are also needed.
We have some worries about this, because although we can't identify the exact problem, we fix it somehow. Any aclaration from your side will lighten us in our journey, so we thank you in advance.
Hello user6197023,
Is it possible that there is already some load on the N5VDC during startup? The LT1054 needs to charge the output capacitor at startup, so if at the same time the LT1964 is discharging the output it will be hard or impossible for the LT1054 to start.
If you can delay the startup of the LT1964 on one of the failing boards and check if this delay helps, this could be the root cause of the issue.
In addition, the output capacitor of the LT1054 should be 10 times bigger than the capacitor connected to CAP+/-, so it is possible that the reduction of this cap to 10uF helps as well.
Hi Brigitte,
we have suspected many times that could be the LT1964, but removing it from the pcb hasn't fix the problem. Do you think it could more probably that the several OPA192 which are connected to N15VDC and P15VDC could cause the N15VDC discharge? The P15VDC is faster than the N15VDC, so I suspected that these components are half-on when the LT1054 wants to start.
I'll try too the input capacitor change, thank you!
Hello user6197023,
And please reduce the flying capacitor to 10uF (this is the cap connected between CAP+ and CAP-).
What happens on a board that does not start if your remove the OPA192? First one, then another one, ... Does the board start at some point?
Please check on another not starting board, if it helps to remove C275. If this does not help, please remove as well R241.
Brigitte said:Hello user6197023,
And please reduce the flying capacitor to 10uF (this is the cap connected between CAP+ and CAP-).
What happens on a board that does not start if your remove the OPA192? First one, then another one, ... Does the board start at some point?
Please check on another not starting board, if it helps to remove C275. If this does not help, please remove as well R241.
Hi Brigitte,
thank you for your answer. We have solved this issue in some PCBs doing as you said, changing and reducing the number of OPA192 or removing the startup architecture, but we do not see clearly why is the cause of the problem.
Anyway, we have noted all your recommendations, so thank you very much.