Other Parts Discussed in Thread: TPS543620EVM, TPS543620
For the TPS54J061 to generate from 12Vin the following voltages:
- 0.95V or 1.03V (~2A or more) +/-30mV tolerance
- 1.8V (~3.5A or more) +/- 90mV tolerance
- Others such as 1.2V, which is not as stringent in requirement
These two rails has the requirement of low noise with line and load regulation of <0.4% and <1.2% respectively.
the transient response of this part is Ideal. However, considering the switch on time (t_on) at 95ns max especially that we have 12V as input, do you think it is a suitable candidate for these rails?