This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV704: Output Current Limit Transient Response Time

Part Number: TLV704

Hello,

I'd like to place a crowbar circuit on the output of a TLV70433 regulator with 10µF of dedicated output capacitance and 2.2µF of dedicated input capacitance. The output will also have an additional 10µF of capacitance located six inches or so from the regulator and the input will have an additional 10uF within an inch that serves as an output filter component for a buck converter.

Can you elaborate on the output current limit transient response time of the TLV704? I see no mention of this in the datasheet and I'd like to make sure that the fuse in the crowbar circuit is able to reliably activate.

Thank you,

Carter