Hi,
My customer has a question regarding the Vout Tolerance of Webench designs. Wanted to confirm - is the Vout Tolerance in Webench the typical min/max % value? See value below using the TPS62130:
29. Vout Tolerance 1.972 % System Information
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer has a question regarding the Vout Tolerance of Webench designs. Wanted to confirm - is the Vout Tolerance in Webench the typical min/max % value? See value below using the TPS62130:
29. Vout Tolerance 1.972 % System Information
Hi Rakxit,
Thanks for the above query. For this device, WEBENCH calculates Vout tolerance for worst case(Maximum %) by considering Feedback divider resistor tolerance % and Vout accuracy of the device.
Vout accuracy considered for calculation:
Please find the below app note for your reference, Vout tolerance calculation on WEBENCH is similar to this.
http://www.ti.com/lit/an/slva423/slva423.pdf
Vout tolerance for default WEBENCH design for TPS62130 is 2.94% . We could not verify 1.972% mentioned in above post.
Regards,
Shaheen S M