Other Parts Discussed in Thread: BQ25980, , BQ25790
Hi:
I use BQ25882 & BQ25980 solution for 65W charger;Help to confirm the following questions:
1: When 65W fast charging, bq25980 fast charging (input:20V / 3A), bq25882 will enter the OVP protection state, can the path management be used under the protection state? In addition, if the fast charging voltage drops to 5V, OVP, it will recover?
2: Our original plan was to turn off the charging of bq25882 at fast charging (20V / 3A) through IIC and keep the path management function. Can it be realized?
PS:The recommended design is BQ25790&BQ25980
TKS