This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5119: Inquiry about UVLO operation of LM5119.

Part Number: LM5119

Hi, TI expert.

The customer has an inquiry about UVLO operation of LM5119.

- Condition : When forced UVLO off, UVLO off after 321ms Delay by external circuit.

- Questions)

Low Side FET operates intermittently under the condition that UVLO Level is not dropped from 1.2V to 0.4V.

(1CH: Input, 2CH: Output, 3CH: IC UVLO, 4CH: Low Side Gate)

Under the above conditions, UVLO Pin voltage is applied, and it is in Open Loop with Load S/W Off.

It makes sense if the Low Side Gate waveform is maintained or does not appear at all, but the waveform appears like a protection operation.

I wonder why. Is there a specific protection circuit for this?

In addition, there is a schematic with LM5119 applied.

However, because the customer does not want the schematic to be disclosed, please provide your e-mail address. I will send you the schematic.

Please check and answer.

Thank you.