Hello TI,
I designed a flyback SMPS based on the PMP4650.
However, the input voltage operates normally up to about 14V, but if the voltage (about 18V) is raised above that, the operation stops.
The cause of stopping the operation is that the dis/EN signal is high.
Element damage occurs between the base-emitter of Q4 and D14 is burned.
I changed the 33kohm of the R77 to 10kohm. The phenomenon is the same.
What could be the cause?
B. regards
SY