This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65135: Positive and Negative Outputs Smaller than Datasheet Calculations

Part Number: TPS65135

Hi,

I'm using the TPS65135 to generate a +/-2.5V dual supply for a bipolar analog to digital converter. After reviewing the spec sheet, I've chosen R1 = 100kOhm, R2=100kOhm, and R3=200kOhm which should provide me with the proper voltage outputs. All capacitor values used are those supplied in the datasheet (4.7uH and 10uH), with a 2.2uH Inductor. When measuring the voltage, however, I'm only getting +/-2.2V and am not sure why. If it helps, all capacitors used are polarized but are placed properly to account for the needed orientation (cap on negative supply has + on ground, - on output. Cap on positive supply has + on output, - on ground). This circuit is also built on a breadboard. I know breadboards have a very small capacitance between pins, but I figured it wouldn't be enough to see a 10% drop in both outputs from their expected value.

Thanks for your help!

  • Hello Collins,

    Couple of points to note are: the positive output voltage range for this device as specified in the electrical characteristics section of the datasheet is 3V-6V. So 2.5V is outside of the specification of this device.  Also, I am thinking that the grounding scheme will be very poor on a bread board design. For example, center exposed pad of the device is supposed to be connected to a solid PCB copper which you are probably not able to do on the bread board. So I am thinking that this could possibly be contributing to poor regulation.

    Kind Regards,

    Liaqat

  • Ah ok shoot you're right, the 3-6V limitation is probably my biggest issue. Thanks for your help!

  • Hi Collin,

    I am closing this thread for now. If you need further assistance, please respond to this or open another thread.

    Kind Regards,

    Liaqat