Other Parts Discussed in Thread: , EV2400
I am using the bq25120aevm development board. I have a lithium ion battery connected to J7 and a usb 5v charger connected to J3. I have the chip set up to output 1.8V on the SW pin. When I remove the USB charger from J3 with the battery still connected I expect 1.8V to still be present on the SW pin or Vsys. Instead the chip switches and outputs the battery voltage. Do I have one of the registers set wrong. I have not been able to determine what the problem is.
Here are my register settings.
* Created: Sat Jan 30 21:38:46 EST 2021
*
* Format: Register Name tab Character,\t Hexadecimal register value.
* Device: bq25120
* BQZ Container: Charger_1_00-bq25120.bqz
*
Status and ShipMode Control 41
Faults and Fault Masks 00
TS Control and Status Mask 88
Fast Charge Control E8
Termination/Pre-Charge and I2C Address 0E
Battery Voltage Control 78
SYS VOUT Control AA
Load Switch and LDO Control FC
Pushbutton Control 68
ILIM and Battery UVLO Control 3E
Voltage Based Battery Monitor 3C
VIN_DPM and Timers 42