Hey team,
So I wanted to control my EVMs with an external circuit. I checked the schematic and came to the conclusion that one has to remove the switch to connect to the Enable testpoints.
If not, the en1/en2 pin would either be pulled to Vreg or gnd. Ok:
For some reason, if the enable2 pin pulled low, I can still measure an output for the 3.3V, same goes for 5V (en1). I even measured 0.00V potential on enable tp.
Before removing the switch the TPS turned on/off just fine. What am I missing?
Thank you
Karim Bingoel
PS: Selecting a proposed part number above doesn’t work on mobile devices (Safari)