Hi Team,
In the TPS62810-Q1 datasheet, there is an electrical spec for Load Regulation and Line Regulation. Can you help me understand how this is spec'd? For example, the Line Regulation say 0.02%/V.. does that mean if the output is set to 1.1V and my input voltage has a line step of 1V (say from 3.3V to 4.3V), that my output voltage will deviate to 1.1V + 1.1V * 0.0002 = 1.10022V?
Thank you,
Jared