This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi. Help me please to understand why LM25118 isn't working in buck-boost mode. While Vin=24V, required Vout=12V / Iout=2.5A, LM25118 is working in buck mode correctly. But when Vin=10..12V, required Vout=12V / Iout=2.5A, I'm having Vout~<8.5V, Vfb~0.8V. I have tried to change values of external components, add more in/output capacitors, turn off UVLO, but unsuccessfully. Please check my scheme.
Hello Evgenii,
Are you using a 2 layer board or are there more GND layers in the middle? I am asking because with 2 layers, the GND connection is relatively long, especially for the low side transistor on the boost side.
Can you please check at which load the output voltage starts to drop? Please as well compare the real output voltage with the calculated value from the feedback resistors. Is there already a difference at no load?
Hello Evgenii,
As I did not hear back from you, I expect that you have been able to solve the issue and will close the thread now. If this is not the case, please post below or create a new thread if this one is already locked.