Other Parts Discussed in Thread: LM5181, LM5180, SN6501
Hi,
I cannot achieve the required output characteristics. Almost all denominations are calculated according to the datasheet. The transformer is selected close in inductance to the recommended one. What could be the problem?
The transformer is selected based on the size requirements. Perhaps you need to choose another transformer from the LPD3015 line.
In this circuit, I need to have at least 100mA. But now, with a load of 100 Ohm, the voltage drops to 0.2V. This means that the current is about 2mA (0.0004mW) - this is much less than it should be.
Additionally, I attach oscillograms, they suddenly suggest an idea. Large enough needles are visible