Other Parts Discussed in Thread: AM4372,
Hi Power management Support Team,
I have a question about PMIC regarding the following post.
Regarding the connection between AM4372 and TPS65218D0 with the RTC function disabled,
the current customer's schematic is as follows
"Current schematic around the PMIC".
Q1. Is there any problem to modify this schematic as follows.
This setting are referred to the AM437x schematic checklist; Table 2-3 RTC.
-RTC_KALDO_Enn: Any AM437x 1.8 V power supply -> VDDS_RTC
-PMIC_POWER_EN : RTC_PMIC_EN -> NC
Q2. do I need an inductor or some other circuit for the output?
Or can I use a 10kΩ pulldown as I do now?
Q3. What should I pay attention to in connecting AM4372 and TPS65218D0 when I disable the RTC function in other cases?
Q4. As the following thread, the combination of AM4372 and TPS65218D0
should be required the connection in "Powering the AM335x, AM437x, and AM438x with TPS65218D0 user guide"?
This means that RTC disable mode cannot be selected, is this understanding correct?
Best regards,
Kanae