Other Parts Discussed in Thread: BQ28Z610, EV2400
Hello,
I have 3 questions:
1) Can the main CPU send an I2C command to the BQ25883 chip to turn off VSYS? I looked at all registers and I found several VSYS status registers, ADC registers to read VSYS voltage, INT flags, and so on, but none to control its on/off status. I'd like to be able to cut the battery supply voltage to the main circuit when the device is connected to a secondary power input.
2) What voltage will I actually get on VSYS? I'm using 2x 18650 battery cells in series at a BQ28Z610, each cell with ~3.7V. Will I get around twice that value on VSYS (7.4V) when the batteries are fully charged? My circuit follows at the end.
3) Do I have all that I need for the EV2400 on connector N1 (below)? I believe all I need is SCL, SDA and GND, but note that my circuit has no pullups on SCL and SDA.
Thanks!
Eduardo