Other Parts Discussed in Thread: BQ51050B,
Hi everyone,
I designed a PCB that operates with a LiPo battery and charge with wireless charging (bq51050b) . At the very beginning of the circuit I have placed the bq29707 battery protector
https://www.ti.com/lit/ds/symlink/bq2970.pdf?ts=1613323147424&ref_url=https%253A%252F%252Fwww.google.com%252F
According to the datasheet the undervoltage protection level for bq29707 model is 2.8V.
This is the sub-circuit with the battery protector. BT2 is the LiPo battery. Please ignore BT1 (this is for a coin cell battery option)
The circuit works normally and the cutoff level works as expected.. When I finished with the initial test I left the prototype laying around for around a month with the battery connected to it (this is going to be a device with integrated non-removable battery). After this period I decided to make some additional tests and I realized that the battery was drained down to 0V. As a consequence, the wireless charging cannot charge the battery and I have to replace it. I know that batteries have some self-discharge but I am sure that is not the reason behind then drain to the button effect.
Any suggestions? I need to maintain the battery level at least to 2.8V
Thanks in advance
Nick