This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600EVM: UCC25600 Ref Design

Part Number: UCC25600EVM
Other Parts Discussed in Thread: UCC25600, TL431, , UCC256303, PMP20694, UCC27714

Hi,

I'd like to use UCC25600 controller for a low voltage LLC resonant converter application with input 12V and output 6V.

would you please share the part number of the optocoupler used to create isolation between output and RT pin? or please provide the optocoupler specification.

Could you also explain why we need shunt regulator (TL431)? 

  • Hi Ardeshir,

    The opto-coupler part number from the UCC25600EVM is H11AB17A..We've used VO618A in other designs as well.

    The shunt regulator acts as an error amplifier that will adjust the amount of current in the opto-coupler to achieve regulation of the output. 

    Best Regards,

    Ben Lough

  • Hi Ben,

    Thank you for your input. 

    I am currently trying to run simulation with UCC25600; but, it appears that I do not get PWM from GD1 and GD2.

    I ran a simulation weeks ago using TINA TI with the same circuit shown in attached and I was able to get desired output from converter. 

    I downloaded PSpice model of this controller from TI website; and it appears as follow - would you confirm if this Spice model accurate?

  • Please find below schematic of LLC converter and the controller + feedback circuit. 

    For quick validation of controller functionality, I am applying 5V to SS pin and disabled OC for now.


    GD1 and GD2 

  • Please find below - the model in "txt"

     UCC25600
    *****************************************************************************
    * (C) Copyright 2013 Texas Instruments Incorporated. All rights reserved.
    *****************************************************************************
    ** This model is designed as an aid for customers of Texas Instruments.
    ** TI and its licensors and suppliers make no warranties, either expressed
    ** or implied, with respect to this model, including the warranties of
    ** merchantability or fitness for a particular purpose. The model is
    ** provided solely on an "as is" basis. The entire risk as to its quality
    ** and performance is with the customer
    *****************************************************************************
    *
    ** Released by: WEBENCH Design Center, Texas Instruments Inc.
    * Part: UCC25600
    * Date: 25SEP2013
    * Model Type: Transient
    * Simulator: PSPICE
    * Simulator Version: 16.2.0.p001
    * EVM Order Number: EVM (HPA341)
    * EVM Users Guide: SLUU361April 2009
    * Datasheet: SLUS846B SEPTEMBER 2008REVISED JULY 2011
    *
    * Model Version: Final 1.00
    *
    *****************************************************************************
    *
    * Updates:
    *
    * Final 1.00
    * Release to Web
    *
    *****************************************************************************
    *
    * Model Usage Notes:
    *
    * 1. The following features have been modeled
    *      a. Switching Frequency v/s RT resistor
    *      b. Deadtime v/s DT resistor
    * 2. Figure 7, 8, 9, 10, 11 from the datasheet are not modeled (Values at 25C are considered).
    *
    *****************************************************************************
    .SUBCKT UCC25600_TRANS DT OC RT SS VCC GD1 GD2 GND
    $CDNENCSTART
    eee8c5c7a2bc4b01f045f303678664e7916da0bae22e8cb0bba041dd67c69ce448ea70148a9ac1670c8926c1ac5057c8ccfcd77bf87ca9dced52cc602f48c27b
    e9f419af62bfe95e628e6c2a84cc65dd2688e0dfc494de0f519c9500d4b801cf8492e52ca990713717ab25c39b3409a859abfabb00ad70ba53081cfaa9230181
    09a503e1af40f07ab1b2e0ee1c221987aad0cae5ebf3019a4cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a910f86bbc1438841da
    d7a26453a15f2d3fd97dad888f86e675e57c28c1e9a9502d70b6abf7724500c3410acafc9f30454ae73070a45f1d549c6598c49887b4fc2b07012a1a8f02beee
    a24b33ea3c74eb38706b807646b80371a08792b1034404eb202cc2bd77d193d6d76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    6dcc2999c2dfe559706b807646b803714faa76dd4ebef815c5d41ad0cd979521e847dda77d5f94434cc7d4f7427922f33dbf35e2592bf3d72ea50de8f0467f53
    e9f419af62bfe95e08e79cbf8de54de32688e0dfc494de0fded06813055f21138492e52ca990713784abccbe8accc05583f8b3363b98baf2193d33a59583ec31
    b5f1c17ee7956303e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956a2fce07424ad42e8af357abf43b3ebd61
    1ac3d64a7ec42565706b807646b80371507d7052a101b44aa5e41a9333d4c1f5f26d9a015e093696244a25b74d6efdeba792d7c8ab2c4676f92a0f9bacbce411
    dad4b7980b83d60c1db9be5844c9b7c84ec5850e704dd631fbd67efb1043a1e26efcae405adba980ca47c4a8e8c8d49f752925d49cb16d497a3fbd26708b2a8e
    385bb969478bc1fd0070af46a9dd881263eaf61d73c632f1baba462b7c42fb9a7208a85e1aefd30acba88274aa3b76e047bef198f0ea413bb6788c934b887a04
    e9fdfc8a753de1116bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331342b8faa1fa650af416a9a8a27fd2d97fa31bed7b19595e6545cc6ca479f16c6b6
    e9f419af62bfe95e525f4881cdcee43c2688e0dfc494de0f10b9d15db02a3e668492e52ca990713784abccbe8accc055d5048aa8ddca991f86d72bcab6386af3
    bac1cf59d444029c8675a01b2db95be742cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5547c2999a24d1543d33d3c60d69cac8654beef1674d8a7fbe
    e9f419af62bfe95e26b975abe1d7cf1f2688e0dfc494de0f7449fa7747b5c4268492e52ca990713792b35fbc4ba24d2d71f707dff3932ec8988389fcf44dcc43
    7d9a2c7ef247c72daf399d32d282acb6a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c79421cde62a0a842d2d
    e9f419af62bfe95ea3691f164915ef962688e0dfc494de0f0a3d9d17a53346128492e52ca990713774bd84a1f90ee88ca4b6f13b7315f59fce56133b05a358cc
    51a837e5b8d59442e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956a2fce07424ad42e8af357abf43b3ebd61
    32cd76a2a36328a94c640cb94db3c0afb00af8c7ad6033fbb192f6e2cf6745f07a8ee61b2ac7ee78a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    b9d10fcc51398ec8706b807646b80371fb7daec075f10ab94f8181b227c1b6b542cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5501d74eda4c25163d
    e4d6b70bcd676ae4706b807646b80371da398583b1e259ecf9b267a2118cee01fb55a0e22a35a4ae42cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    114fa6e869ae2eeb706b807646b80371a08792b1034404eb125c8738b16ab83779272ff9e6b7246c7e9471621cbe5cc862d766f77596a54b1c022559c34d47a8
    e9f419af62bfe95e6af56f2fcb564d812688e0dfc494de0fbe98d310e4b8710b8492e52ca990713774bd84a1f90ee88ca60707c345db8c532a10ec055f853139
    bac1cf59d444029c8675a01b2db95be742cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5547c2999a24d1543d33d3c60d69cac8654beef1674d8a7fbe
    4374777403e0317e706b807646b80371a08792b1034404eb1822436578af3579d76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    c13b7ed85c9af80d706b807646b803716afbd30163cc0e01e9d468469750e39100d3e0b087c7374442cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    782515cfeeba6caa706b807646b80371a08792b1034404ebc25c48964feba766a61640f12b3724f2b153c27adf9daee400d3e0b087c7374431d019cdae70d870
    4098a1f977e327a0706b807646b80371e6cf343378ade772dc60fa02592d74defaeaa281e22d723e644126c9831a96bd4cc7d4f7427922f3c6cdf92ae4ff7b62
    6fd49a40a2a874a2706b807646b80371e0d235006df12fb4faca85d0862a74fbdaa3793c72e7d69fb62ae495d8bbcdb54b5e7ad1285a439c6f3d9f23e79cb879
    8ed84cd0180fcacf706b807646b803710609a13501132a863ae2468b9ecaccb91db9be5844c9b7c84ec5850e704dd631fbd67efb1043a1e2d4ad0c203b8ad9ef
    e9f419af62bfe95e34c73dcbf92dd8722688e0dfc494de0ff5b614c6d43fc5148492e52ca990713774bd84a1f90ee88c70ea3b4af5e7d669135920380e06a9e4
    53c082b195825f91eeb858a3a69e92dd644126c9831a96bd4cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a910f86bbc1438841da
    3e2f6d3b6fa1f79e42cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5547c2999a24d1543d33d3c60d69cac86528e7d71460b9c154901d3f3c7f1ef60e
    d29a3819b03a632a706b807646b803717150993bfda44d1190770f01880100d722b9300ae6b7e53ea2c537184c69296512643236dcc925be9d6bedf9d0034ac8
    cc4ebde65d14696797834113c2b271e8d2693a7076e1e42ecc4010cbb1111118e31b524cc0fa8723463c40b2f9559a061db9be5844c9b7c87d7eb54abcbf2b3f
    a640afca273b027d706b807646b80371a08792b1034404eb23a2f9e11fce1bde9cecdce65f97422fef1d7357d3c4e2f3644126c9831a96bda118e546bf58ab2c
    5125ca7103a1d6ba706b807646b80371a08792b1034404ebf37ba79774a7028ac64d81576cf5798f00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    e9f419af62bfe95ea84ecbc7159c51ad2688e0dfc494de0fc60e3c5ac968ec44749d13634498f34bc9322890ded6647b92bdf4561000be04db94e8b8c3713864
    9d80d756e6e49498df838cad64f56a21a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c79421cde62a0a842d2d
    0014955abd37d950dc14d9a6d715e693c6ea45c1dc497e4be9fdfc8a753de1116bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331347930dd0ea548b5c0
    492b5dc666856a64706b807646b80371a08792b1034404ebc311f70181f567225a54ab7d3964534c640b08cecbb6cffe042f0c0c78bb0deb673b81ca19be4e33
    385bb969478bc1fdbe53f7f0fcc00df7913aa1dcb20716bebaba462b7c42fb9a7208a85e1aefd30aa61dbc6176f11e29c7c0ff6aff14e47c5f4f205501a14c16
    af399d32d282acb6a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c7941d4e7946c3b9e444765a78faae22ede9
    1d8e0afd88a08353706b807646b80371a08792b1034404eb3352a90b39e0fd4f42b44158b08ce2af478a87bc5b8e6cf96bf55428c35ad9f811e89b3f90b53f1c
    69ff18044fae7c89706b807646b803714faa76dd4ebef8157b583f31c5e2f595ee296b5d6cfe99f66598c49887b4fc2b7857de061e2a26efee079f887bcd36bf
    a7955988c1a00c21706b807646b8037178bd4ed1634daf7a4f8181b227c1b6b542cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5501d74eda4c25163d
    ed86d06aaca96870706b807646b803710f5a44c8cfeac7e10127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    62df88c5a2e359bf706b807646b80371a08792b1034404eb1c2c68874e4eae6bc6a72b5bd58772bc50932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    9ed7c1c1396d1611706b807646b8037176e9956d52804abebafe5040957ee65200d3e0b087c7374442cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    1772a44faf4c4234706b807646b803710be92d880872d2740127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    9ebb400152663803706b807646b80371a08792b1034404eb69c3e87dc25a3991ca9fe2167b6d55f1f21bc70cf01660c262d766f77596a54b1c022559c34d47a8
    16329a8c0d160517706b807646b803719fe95eafa8359aaffde8bf6b1edbbb5af618abeb8f40b31e710f626c2faf14a6e033578534f961d21e23b55ace376035
    385bb969478bc1fdcfa6616042166ac248b855340200e68f5aa6f74fa8c7012466eaeb9fc4cc8ae1b6ab3a18e872196fa2c86709dd4ed6558482087c193a8f13
    55136b92d0559ec4e71f71e1875841714cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a91de6ccc763475b3ceb88a6c9366dff5dc
    e9f419af62bfe95e5bd1d958b85c63372688e0dfc494de0f351c48fd3cc0b02c8492e52ca990713774bd84a1f90ee88c11379f40f6945fe7cfc8f60bb1e4b77a
    53c082b195825f91eeb858a3a69e92dd644126c9831a96bd4cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a910f86bbc1438841da
    3e2f6d3b6fa1f79e42cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5547c2999a24d1543d33d3c60d69cac86528e7d71460b9c154901d3f3c7f1ef60e
    c3f79b4609191d9b706b807646b803717b6b96cab45c6ee93ae2468b9ecaccb91db9be5844c9b7c84ec5850e704dd631fbd67efb1043a1e2d4ad0c203b8ad9ef
    385bb969478bc1fd99833895c09d905397834113c2b271e8baba462b7c42fb9a7208a85e1aefd30a06e21ba87059f379b264866b3f10c5af4576120197e38a69
    af399d32d282acb6a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c7941d4e7946c3b9e444765a78faae22ede9
    d2a6f7e632f6e240706b807646b80371665aaae256219221d76167baccb438ba00d3e0b087c7374442cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    bdadeec1d4eda933706b807646b80371a08792b1034404ebfda371680e0c013116f9a635cd037322bafe5040957ee65200d3e0b087c7374431d019cdae70d870
    c18beea1ddade083706b807646b80371a08792b1034404eb55e2a0cb857e7be44ba2216b7e828e5b00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    88642418aa31eccb706b807646b80371a08792b1034404eb104f5bc60495b9f82509998b8b3441b9bafe5040957ee65200d3e0b087c7374431d019cdae70d870
    e9f419af62bfe95eddb4b29aaeb56c852688e0dfc494de0f23d421d6f72d6ab08492e52ca990713774bd84a1f90ee88ca4b6f13b7315f59fce56133b05a358cc
    51a837e5b8d59442e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956a2fce07424ad42e8af357abf43b3ebd61
    32cd76a2a36328a9bd8a91623ed6cdbab00af8c7ad6033fbb192f6e2cf6745f07a8ee61b2ac7ee78a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    c768dd54c070d682706b807646b80371a08792b1034404ebea249048f89233184c0be7416ff9fbc856ed27f701de477562d766f77596a54b1c022559c34d47a8
    faf38c75316d0585706b807646b803717af6f4c6b03f4e16c8459af3f01fecbddc98bcd7ae1314f8a263d3ef9a2264bd7386463fc26a014a5237ed7e51143eec
    e9f419af62bfe95e09c4739f84a8c1c02688e0dfc494de0f7d23116f74ca45da8492e52ca990713774bd84a1f90ee88cefd852fe6c1aefeca5cd6230ab7f846f
    172fcef26330567ff44496155f03ed4f5651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    1b321580e3e7edcf706b807646b80371ca734aa83b8f8426e9d468469750e39100d3e0b087c7374442cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    f609c441bb61e78c706b807646b803714b1c4df981679e1dc79c5195b3c697fd042f0c0c78bb0deba263d3ef9a2264bd7386463fc26a014a5237ed7e51143eec
    e9d36920d2449dc8706b807646b80371a08792b1034404eb677d49eb2b9eed9f8b91ababefd8c706bafe5040957ee65200d3e0b087c7374431d019cdae70d870
    025af1404b9bbe0d706b807646b80371a08792b1034404ebdd4c62910e4aa482a984b5c814f142dfbadae1317df5ab3f23b782b3d6a37df184ed6abb421c1f02
    e359198f0d54dd04706b807646b80371a08792b1034404eb22e712c6dfe7eccad76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    5aa875be979324eb706b807646b803714faa76dd4ebef8156e56ef7b103a718f6bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331347930dd0ea548b5c0
    174aab22bc8b48c3706b807646b80371a08792b1034404ebb3a34c493507b4faaf4b7be9fedfc9a8478a87bc5b8e6cf96bf55428c35ad9f811e89b3f90b53f1c
    f55d627e5b6a5781706b807646b803710cd21e8ca845a98b0127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    f9d40bfe034dc9e4706b807646b80371a08792b1034404eba05659ea5c1551414fa6130fb0de8c9350932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    8df0563ff6b12bcb706b807646b803714faa76dd4ebef815e3c8854d9eba907f1d4e452fee093da4e033578534f961d26e9adfbcaaf6fe51c173022dc07b974d
    638ff464aec55f37706b807646b803715a6fa533133f11a3e5ed36f61e63f360c226e28d6958f7095651d10d29ebe89e9cd1b241aee3ca524f90023d786d0eaf
    f24cff2bb787655c706b807646b80371701dd54135e2845d7c63738b614a4dc1d0b01a738ef93a9d303d7240d8c3139de033578534f961d21e23b55ace376035
    fb084946fa1d2f48706b807646b803715671e59bd39a227305d2793e5127767ae07746d3d0076eb200d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    e11f20ad36e7e098706b807646b80371eeab2e0253cc6f8753823fed859af48366eaeb9fc4cc8ae15bcb4f3deed2fe5882b5425599ed1844b97ac6965124046b
    ebf1591b7680bc626bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331342b8faa1fa650af416a9a8a27fd2d97fa31bed7b19595e6545cc6ca479f16c6b6
    5b163e195ceeae4a706b807646b803715671e59bd39a22730b45656f6126dbeaae8ece02dda0bcfd60877ff0912fae9e6598c49887b4fc2b07012a1a8f02beee
    da32fce65bd9e4ea706b807646b80371bd8ecf3ecfc8ef6714361fb5d99f43506bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331347930dd0ea548b5c0
    4cda0bfb3e7f17e6f60b46ee8e8166be448af6bd68b1383883f4586e2fcc0a634e237b59546ef6f22962ea8ee267008d644126c9831a96bda118e546bf58ab2c
    064c7d10b22fd68aec4b5a01552036e1303f53704e2595d18fe1aec0698a9b90d3b99b01fef3c64498c453163ff10bcfe4b2500fe4e809c5769ab468c6f113f9
    70c9126bd9ff8882e9aa8206dccedec85651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    c930ee9bd4ca2400e26ef9f44a7eb3b5ca023470191575ccfc301e5086eb985396b3eacb99bc6a95a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    064c7d10b22fd68a472daf882b741cd8fd9475d1df4fab6d2ff3983901ebdf1bfaca85d0862a74fb0c76c4db3c95135f9dd5ccfa588ebff3bb6b2bcf56be112b
    ad70a4fb8ff671b66bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331342b8faa1fa650af416a9a8a27fd2d97fa31bed7b19595e6545cc6ca479f16c6b6
    32cd76a2a36328a92532381493787cb8d6600d5af11a4d3eb1840a4bfbabe1c93f013fb7ee415b211b4ad6a9271e801ed4155cda969bd8d9fb1b1de5b0925d59
    46ca60d9e0a03ec1cfe1d30080fa8985e3570c3308686a4dbe7209490363213f45e4e160e3aa04d7a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    9eaf82adc2a1140d34c73dcbf92dd8729c4005bcd9ca79e6e00eefbd63f1d45d8492e52ca99071373360b3b2bcd4874aef23bbe4f31b58a8673b81ca19be4e33
    8e12dea80c549de261698f310be5a400f78f01ca7cd3184ca95fd1712bcaf1b029b48a33a73df9caaf399d32d282acb6a263d3ef9a2264bd73ac5403918b2efd
    928d7a9f462cf2ed706b807646b8037150eb858f9032cc838b0547476f2f18a15d4b44c85b70670f7e695e5d531063625a4c9a26c2a42486b77986be7141a48f
    1b6bebc0bc33482c706b807646b80371bd8ecf3ecfc8ef6745b5a70a5cc0245b5651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802e323c1799b4666e62
    07c82d144c68cf87cd9f9b0fe66d8ad11aedfeffe85ebe258d915cdb7782fd416598c49887b4fc2b7857de061e2a26efa85bfcd7236670cdeb605ebf76f26de2
    1632a67cf5c03a1a706b807646b803717c63738b614a4dc1deb29c76e244f6ee66eaeb9fc4cc8ae15bcb4f3deed2fe58f20766bdac48276ea80c2743bc5ec9e0
    f0acca179947ec8f6dba65afb526cbc1a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c79421cde62a0a842d2d
    f57b0f2f4f3d276e706b807646b80371eeab2e0253cc6f8774a1258979547e3db7e56e956fec2f26ef1d7357d3c4e2f3644126c9831a96bda118e546bf58ab2c
    593e80cc430081d2706b807646b803710b45656f6126dbea8ba75e1a7d67df4598edc312c449029b94ef342977743ad062d766f77596a54b1c022559c34d47a8
    d6aca196616365d3706b807646b80371eeab2e0253cc6f877ffffa9baf890d4866eaeb9fc4cc8ae11b9fb80fc79e7cd8b529248e59261b2c62b84e5bac7fe806
    290ad72d9c5d86d6d5ba6b0a204ed1235651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    9209d3ab4a447b3e0529bb43a7ec9944cbc940513e636f1e7a8ee61b2ac7ee7875398a5ed1f1b9156bf55428c35ad9f818b1e200d5b367e949f39e38b6c0fccc
    bdd8d6b45d26c9f3706b807646b80371143f62011610c8e26de7d7947cf2bfa76bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331347930dd0ea548b5c0
    b965afc66411a939706b807646b80371fe2486f8cdb753dd8fa9d028134572658df8cf962e0b71f650932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    064c7d10b22fd68ad6451f700dbd4eeafd9475d1df4fab6d5829074c65631300d3b99b01fef3c6449b399e078b2806b680890c5e795f5da7f08aa6603ffcf1aa
    a8835ce432d01b0c1db9be5844c9b7c84ec5850e704dd631fbd67efb1043a1e26efcae405adba980ca47c4a8e8c8d49f752925d49cb16d497a3fbd26708b2a8e
    32cd76a2a36328a92532381493787cb8c7c0ff6aff14e47c073d57a0eaa16b2e60c9783cd34f18105960294be34dfb0c61698f310be5a400c99cc804ae839bdf
    fd6bb2445a39ab416598c49887b4fc2b7857de061e2a26efa85bfcd7236670cd3e51762787380085b0f5c467238a30432f65f2e99cc333ed7cdf306a4c574167
    71011f181f54b3e361ad8839db814189a8d6984e08c7aad08bf4f6f2e78aa0a8b9b3abf75e62eaab52e00aa790b455bb3c185b56871dcecb3b300708695416e3
    a7016332727eeac3706b807646b80371eeab2e0253cc6f876d84478bc105beae23ae7ba6d36cc4bd50932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    9f337bb24085865c706b807646b803710b45656f6126dbea2c26e93bf2541112a43dc3d884d87a691962f61c1a635c8d62d766f77596a54b1c022559c34d47a8
    80b5fda8ff9d3f4e706b807646b80371fe2486f8cdb753dd857295c9975dd8465f1937206921a2ed640b08cecbb6cffe042f0c0c78bb0deb673b81ca19be4e33
    064c7d10b22fd68a7509c136893a3e2e303f53704e2595d1e5e7fade4086c0d1d3b99b01fef3c64498c453163ff10bcfe4b2500fe4e809c5769ab468c6f113f9
    70c9126bd9ff8882e9aa8206dccedec85651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    c930ee9bd4ca2400e26ef9f44a7eb3b5ca023470191575ccfc301e5086eb985396b3eacb99bc6a95a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    88070a17816250e7706b807646b803710b45656f6126dbead22a2727f10326dfd76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    25dadebd820afd72706b807646b80371989d190a69797eee0127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    76c226c74162658e706b807646b803710b45656f6126dbeae398f727c47c7615b41429200bc9d6b4cb05648a7343990262d766f77596a54b1c022559c34d47a8
    090e4b6528d980ae706b807646b8037115deb1a5e6728cf5143f62011610c8e2f2fd3f0f55709a15303d7240d8c3139de033578534f961d21e23b55ace376035
    9eaf82adc2a1140daf62c7e801e29edb9c4005bcd9ca79e65e53eb09280546c98492e52ca990713774bd84a1f90ee88c146628815e2daa418b8f92ada6ab6779
    88f02d15ca9c6f41e73070a45f1d549c6598c49887b4fc2b7857de061e2a26efa85bfcd7236670cd3e51762787380085b0f5c467238a30436445e6c14ba2c5fa
    58cf452d198b3802706b807646b803713ccc9fb8d5c7e25e7c63738b614a4dc13a12794a0bbb04c2303d7240d8c3139de033578534f961d21e23b55ace376035
    709cd66b96967eeb706b807646b803710b45656f6126dbeada88a3aa1e8e53f6d76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    8818260e40cfae59706b807646b803712549b74dc22585560127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    afb57ee19c9d50ea706b807646b80371143f62011610c8e2ae1e8de5e31346c1805f3dc1f93d56fe7e695e5d53106362e085717002817eb3117c43488ffc6d6b
    76777896a7ce37a2706b807646b80371debee9ea7afb849e0127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    3d875a9a87f9d624706b807646b803710b45656f6126dbeaf6250f7e15a5c10cd76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    9eaf82adc2a1140d976633e3a662b0a89c4005bcd9ca79e6894381d170438d328492e52ca990713774bd84a1f90ee88c5250164eead6fad4133faeaa1ac7e1ab
    55136b92d0559ec4e71f71e1875841714cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a91de6ccc763475b3ceb88a6c9366dff5dc
    8e641f8c2424c2e1706b807646b80371a97b765744e54e1826d0fbb139962a0b478a87bc5b8e6cf96bf55428c35ad9f818b1e200d5b367e949f39e38b6c0fccc
    9eaf82adc2a1140dcd9f9b0fe66d8ad1e3b798de2a9b9eecaa2f1d7584e4b8d2ce5ec34e6f8ad1ca09a503e1af40f07a6933223ff0a8eca47cf023c2239db233
    7c6a057502825b8b6bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331342b8faa1fa650af416a9a8a27fd2d97fa31bed7b19595e6545cc6ca479f16c6b6
    40f41cdf5245bcc08f8d74c047af5be8387e82ba91c98af427876424abadc0a7280a3d8e4636feaa53456d9034a59a02e827ca08aceff3d79c7a4bc0de56f663
    9eaf82adc2a1140d5bd1d958b85c63379c4005bcd9ca79e6d58cdad0fec876c48492e52ca990713774bd84a1f90ee88c5dba07e1efa84051940d46f618ddb284
    a63f11eaaca09401b5f1c17ee7956303e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956af92be55228ec5c32
    3f2d39c3473bdd81706b807646b803710b45656f6126dbeaa7ac554b70945d8dc82ab3b2f8f47edb53a4999cf475b1ba62d766f77596a54b1c022559c34d47a8
    064c7d10b22fd68a0fb9a87d5a97a04b3d59dfa5c6e6246c6342ce344f4132ecfaca85d0862a74fb5589c49a9624f695cda4baa068a73fff6f6620a49d5db2bb
    ca7f88d3b0d2438ab5f1c17ee7956303e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956af92be55228ec5c32
    80409ca1121b04d7706b807646b803713ccc9fb8d5c7e25e74dc3a64e1e990ed478a87bc5b8e6cf96bf55428c35ad9f818b1e200d5b367e949f39e38b6c0fccc
    92491360359d2ac4706b807646b803717c63738b614a4dc1ede42e8a91db457b66eaeb9fc4cc8ae15bcb4f3deed2fe584430a7a5b441e4d3a80c2743bc5ec9e0
    5f1937206921a2ed7856c6afe220f6455651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    430882ca1e45ea8b706b807646b803710b45656f6126dbeaffb1728fb299b3c25c702c3de286e0aac1cb60b9845d858e24fdfd9bb2e10b0766f5d7227ff3c671
    a155848e3bbce6f3706b807646b803710b45656f6126dbea54054943b5fb4f1ad76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    e713cfefd199f1eb706b807646b80371fe2486f8cdb753dd2b0e7197a01f581383a1af2b064b63d950932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    2b3f0796f933b05af60b46ee8e8166bed102992399a397df1ede05ad024319068bcc8a7f6eba11314e3b5b908c2815ff5651d10d29ebe89e70605af949aa2245
    9eaf82adc2a1140d752f7113017609339c4005bcd9ca79e6026a90a9bc342ef78492e52ca990713774bd84a1f90ee88cf2bc79891bc1c93fd9997f6750464469
    a63f11eaaca09401b5f1c17ee7956303e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956af92be55228ec5c32
    e07dfe0d2e28b89c706b807646b803710b45656f6126dbea58e99fd91daf668a81def0c67df4b206955f478f324f6d7f24fdfd9bb2e10b0766f5d7227ff3c671
    09a7c1f8b05a8ac1706b807646b803717c63738b614a4dc11bfbffa661b63638691018eed3b49c3685d8806da1e0ac981625a916457b09524c721f1915d81d71
    d177348d2deab5c2706b807646b803715671e59bd39a2273715ee7be0cf2a78ffaeaa281e22d723e644126c9831a96bd0913a741f2f1d533dcfb55a634b33adb
    60c9783cd34f1810706b807646b80371e5494a25d92d58bfaad0cae5ebf3019a0913a741f2f1d533c167b19f5561b8d10a3dca7c9f0c7a1a07ca2e46d08f789f
    9af710ac7afcd4a8706b807646b803716d2b3ea68bf556be6f351d1b39770686478a87bc5b8e6cf9691018eed3b49c3685d8806da1e0ac982c66f1c690743c90
    fab9cf2b7c040381706b807646b8037150eb858f9032cc830277ed7ba7f99963691018eed3b49c3685d8806da1e0ac981625a916457b09524c721f1915d81d71
    be52e6aa176ef44b706b807646b8037115deb1a5e6728cf50b95d65fc212ad34478a87bc5b8e6cf9691018eed3b49c3685d8806da1e0ac982c66f1c690743c90
    b29471f7f94cc38f706b807646b80371b10f4f7d78547f3a0127ad895999246523b782b3d6a37df130cb792a729d977e348481f601fee253f54692846f76b1c0
    0b22eb7d0b342b1c706b807646b8037115deb1a5e6728cf5eb7d47e44bd5ce9f478a87bc5b8e6cf9691018eed3b49c3685d8806da1e0ac982c66f1c690743c90
    3e761c6835cdd8d5706b807646b803717c63738b614a4dc15906b005a38828e7691018eed3b49c3685d8806da1e0ac981625a916457b09524c721f1915d81d71
    7d39dd9f81bbcdfd706b807646b803715671e59bd39a22731c90425132b9714749bcb2e9b7241eb4644126c9831a96bd0913a741f2f1d533dcfb55a634b33adb
    f850674c77dc0a72706b807646b80371701dd54135e2845db5a5d7fe347b969f478a87bc5b8e6cf9691018eed3b49c3685d8806da1e0ac982c66f1c690743c90
    93d3808648446fd7a60fd3951de4fe94b6c36883137f300162d766f77596a54b693b06cb62c8947be6b9412e4bab9f0a8218fbb9c051aaeb0d4817371b05d633
    $CDNENCFINISH
    .ENDS UCC25600_TRANS

  • Hi Ardeshir,

    What is the voltage you see on the RT and DT pins?

    Best Regards,

    Ben Lough

  • Hi Ben,

    I do see 2.5V om RT pin and 2.25V on DT pin.

    Regards,

    Ardy 

  • Is the Pspice model okay? is it jumbled? please see below in bolded.

    SUBCKT UCC25600_TRANS DT OC RT SS VCC GD1 GD2 GND
    $CDNENCSTART
    eee8c5c7a2bc4b01f045f303678664e7916da0bae22e8cb0bba041dd67c69ce448ea70148a9ac1670c8926c1ac5057c8ccfcd77bf87ca9dced52cc602f48c27b
    e9f419af62bfe95e628e6c2a84cc65dd2688e0dfc494de0f519c9500d4b801cf8492e52ca990713717ab25c39b3409a859abfabb00ad70ba53081cfaa9230181
    09a503e1af40f07ab1b2e0ee1c221987aad0cae5ebf3019a4cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a910f86bbc1438841da
    d7a26453a15f2d3fd97dad888f86e675e57c28c1e9a9502d70b6abf7724500c3410acafc9f30454ae73070a45f1d549c6598c49887b4fc2b07012a1a8f02beee
    a24b33ea3c74eb38706b807646b80371a08792b1034404eb202cc2bd77d193d6d76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    6dcc2999c2dfe559706b807646b803714faa76dd4ebef815c5d41ad0cd979521e847dda77d5f94434cc7d4f7427922f33dbf35e2592bf3d72ea50de8f0467f53
    e9f419af62bfe95e08e79cbf8de54de32688e0dfc494de0fded06813055f21138492e52ca990713784abccbe8accc05583f8b3363b98baf2193d33a59583ec31
    b5f1c17ee7956303e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956a2fce07424ad42e8af357abf43b3ebd61
    1ac3d64a7ec42565706b807646b80371507d7052a101b44aa5e41a9333d4c1f5f26d9a015e093696244a25b74d6efdeba792d7c8ab2c4676f92a0f9bacbce411
    dad4b7980b83d60c1db9be5844c9b7c84ec5850e704dd631fbd67efb1043a1e26efcae405adba980ca47c4a8e8c8d49f752925d49cb16d497a3fbd26708b2a8e
    385bb969478bc1fd0070af46a9dd881263eaf61d73c632f1baba462b7c42fb9a7208a85e1aefd30acba88274aa3b76e047bef198f0ea413bb6788c934b887a04
    e9fdfc8a753de1116bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331342b8faa1fa650af416a9a8a27fd2d97fa31bed7b19595e6545cc6ca479f16c6b6
    e9f419af62bfe95e525f4881cdcee43c2688e0dfc494de0f10b9d15db02a3e668492e52ca990713784abccbe8accc055d5048aa8ddca991f86d72bcab6386af3
    bac1cf59d444029c8675a01b2db95be742cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5547c2999a24d1543d33d3c60d69cac8654beef1674d8a7fbe
    e9f419af62bfe95e26b975abe1d7cf1f2688e0dfc494de0f7449fa7747b5c4268492e52ca990713792b35fbc4ba24d2d71f707dff3932ec8988389fcf44dcc43
    7d9a2c7ef247c72daf399d32d282acb6a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c79421cde62a0a842d2d
    e9f419af62bfe95ea3691f164915ef962688e0dfc494de0f0a3d9d17a53346128492e52ca990713774bd84a1f90ee88ca4b6f13b7315f59fce56133b05a358cc
    51a837e5b8d59442e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956a2fce07424ad42e8af357abf43b3ebd61
    32cd76a2a36328a94c640cb94db3c0afb00af8c7ad6033fbb192f6e2cf6745f07a8ee61b2ac7ee78a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    b9d10fcc51398ec8706b807646b80371fb7daec075f10ab94f8181b227c1b6b542cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5501d74eda4c25163d
    e4d6b70bcd676ae4706b807646b80371da398583b1e259ecf9b267a2118cee01fb55a0e22a35a4ae42cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    114fa6e869ae2eeb706b807646b80371a08792b1034404eb125c8738b16ab83779272ff9e6b7246c7e9471621cbe5cc862d766f77596a54b1c022559c34d47a8
    e9f419af62bfe95e6af56f2fcb564d812688e0dfc494de0fbe98d310e4b8710b8492e52ca990713774bd84a1f90ee88ca60707c345db8c532a10ec055f853139
    bac1cf59d444029c8675a01b2db95be742cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5547c2999a24d1543d33d3c60d69cac8654beef1674d8a7fbe
    4374777403e0317e706b807646b80371a08792b1034404eb1822436578af3579d76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    c13b7ed85c9af80d706b807646b803716afbd30163cc0e01e9d468469750e39100d3e0b087c7374442cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    782515cfeeba6caa706b807646b80371a08792b1034404ebc25c48964feba766a61640f12b3724f2b153c27adf9daee400d3e0b087c7374431d019cdae70d870
    4098a1f977e327a0706b807646b80371e6cf343378ade772dc60fa02592d74defaeaa281e22d723e644126c9831a96bd4cc7d4f7427922f3c6cdf92ae4ff7b62
    6fd49a40a2a874a2706b807646b80371e0d235006df12fb4faca85d0862a74fbdaa3793c72e7d69fb62ae495d8bbcdb54b5e7ad1285a439c6f3d9f23e79cb879
    8ed84cd0180fcacf706b807646b803710609a13501132a863ae2468b9ecaccb91db9be5844c9b7c84ec5850e704dd631fbd67efb1043a1e2d4ad0c203b8ad9ef
    e9f419af62bfe95e34c73dcbf92dd8722688e0dfc494de0ff5b614c6d43fc5148492e52ca990713774bd84a1f90ee88c70ea3b4af5e7d669135920380e06a9e4
    53c082b195825f91eeb858a3a69e92dd644126c9831a96bd4cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a910f86bbc1438841da
    3e2f6d3b6fa1f79e42cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5547c2999a24d1543d33d3c60d69cac86528e7d71460b9c154901d3f3c7f1ef60e
    d29a3819b03a632a706b807646b803717150993bfda44d1190770f01880100d722b9300ae6b7e53ea2c537184c69296512643236dcc925be9d6bedf9d0034ac8
    cc4ebde65d14696797834113c2b271e8d2693a7076e1e42ecc4010cbb1111118e31b524cc0fa8723463c40b2f9559a061db9be5844c9b7c87d7eb54abcbf2b3f
    a640afca273b027d706b807646b80371a08792b1034404eb23a2f9e11fce1bde9cecdce65f97422fef1d7357d3c4e2f3644126c9831a96bda118e546bf58ab2c
    5125ca7103a1d6ba706b807646b80371a08792b1034404ebf37ba79774a7028ac64d81576cf5798f00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    e9f419af62bfe95ea84ecbc7159c51ad2688e0dfc494de0fc60e3c5ac968ec44749d13634498f34bc9322890ded6647b92bdf4561000be04db94e8b8c3713864
    9d80d756e6e49498df838cad64f56a21a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c79421cde62a0a842d2d
    0014955abd37d950dc14d9a6d715e693c6ea45c1dc497e4be9fdfc8a753de1116bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331347930dd0ea548b5c0
    492b5dc666856a64706b807646b80371a08792b1034404ebc311f70181f567225a54ab7d3964534c640b08cecbb6cffe042f0c0c78bb0deb673b81ca19be4e33
    385bb969478bc1fdbe53f7f0fcc00df7913aa1dcb20716bebaba462b7c42fb9a7208a85e1aefd30aa61dbc6176f11e29c7c0ff6aff14e47c5f4f205501a14c16
    af399d32d282acb6a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c7941d4e7946c3b9e444765a78faae22ede9
    1d8e0afd88a08353706b807646b80371a08792b1034404eb3352a90b39e0fd4f42b44158b08ce2af478a87bc5b8e6cf96bf55428c35ad9f811e89b3f90b53f1c
    69ff18044fae7c89706b807646b803714faa76dd4ebef8157b583f31c5e2f595ee296b5d6cfe99f66598c49887b4fc2b7857de061e2a26efee079f887bcd36bf
    a7955988c1a00c21706b807646b8037178bd4ed1634daf7a4f8181b227c1b6b542cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5501d74eda4c25163d
    ed86d06aaca96870706b807646b803710f5a44c8cfeac7e10127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    62df88c5a2e359bf706b807646b80371a08792b1034404eb1c2c68874e4eae6bc6a72b5bd58772bc50932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    9ed7c1c1396d1611706b807646b8037176e9956d52804abebafe5040957ee65200d3e0b087c7374442cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    1772a44faf4c4234706b807646b803710be92d880872d2740127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    9ebb400152663803706b807646b80371a08792b1034404eb69c3e87dc25a3991ca9fe2167b6d55f1f21bc70cf01660c262d766f77596a54b1c022559c34d47a8
    16329a8c0d160517706b807646b803719fe95eafa8359aaffde8bf6b1edbbb5af618abeb8f40b31e710f626c2faf14a6e033578534f961d21e23b55ace376035
    385bb969478bc1fdcfa6616042166ac248b855340200e68f5aa6f74fa8c7012466eaeb9fc4cc8ae1b6ab3a18e872196fa2c86709dd4ed6558482087c193a8f13
    55136b92d0559ec4e71f71e1875841714cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a91de6ccc763475b3ceb88a6c9366dff5dc
    e9f419af62bfe95e5bd1d958b85c63372688e0dfc494de0f351c48fd3cc0b02c8492e52ca990713774bd84a1f90ee88c11379f40f6945fe7cfc8f60bb1e4b77a
    53c082b195825f91eeb858a3a69e92dd644126c9831a96bd4cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a910f86bbc1438841da
    3e2f6d3b6fa1f79e42cdae931a3d3892c02d2d9372c03ffa79ab8f2b53c66d5547c2999a24d1543d33d3c60d69cac86528e7d71460b9c154901d3f3c7f1ef60e
    c3f79b4609191d9b706b807646b803717b6b96cab45c6ee93ae2468b9ecaccb91db9be5844c9b7c84ec5850e704dd631fbd67efb1043a1e2d4ad0c203b8ad9ef
    385bb969478bc1fd99833895c09d905397834113c2b271e8baba462b7c42fb9a7208a85e1aefd30a06e21ba87059f379b264866b3f10c5af4576120197e38a69
    af399d32d282acb6a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c7941d4e7946c3b9e444765a78faae22ede9
    d2a6f7e632f6e240706b807646b80371665aaae256219221d76167baccb438ba00d3e0b087c7374442cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    bdadeec1d4eda933706b807646b80371a08792b1034404ebfda371680e0c013116f9a635cd037322bafe5040957ee65200d3e0b087c7374431d019cdae70d870
    c18beea1ddade083706b807646b80371a08792b1034404eb55e2a0cb857e7be44ba2216b7e828e5b00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    88642418aa31eccb706b807646b80371a08792b1034404eb104f5bc60495b9f82509998b8b3441b9bafe5040957ee65200d3e0b087c7374431d019cdae70d870
    e9f419af62bfe95eddb4b29aaeb56c852688e0dfc494de0f23d421d6f72d6ab08492e52ca990713774bd84a1f90ee88ca4b6f13b7315f59fce56133b05a358cc
    51a837e5b8d59442e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956a2fce07424ad42e8af357abf43b3ebd61
    32cd76a2a36328a9bd8a91623ed6cdbab00af8c7ad6033fbb192f6e2cf6745f07a8ee61b2ac7ee78a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    c768dd54c070d682706b807646b80371a08792b1034404ebea249048f89233184c0be7416ff9fbc856ed27f701de477562d766f77596a54b1c022559c34d47a8
    faf38c75316d0585706b807646b803717af6f4c6b03f4e16c8459af3f01fecbddc98bcd7ae1314f8a263d3ef9a2264bd7386463fc26a014a5237ed7e51143eec
    e9f419af62bfe95e09c4739f84a8c1c02688e0dfc494de0f7d23116f74ca45da8492e52ca990713774bd84a1f90ee88cefd852fe6c1aefeca5cd6230ab7f846f
    172fcef26330567ff44496155f03ed4f5651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    1b321580e3e7edcf706b807646b80371ca734aa83b8f8426e9d468469750e39100d3e0b087c7374442cdae931a3d3892c02d2d9372c03ffa69f63e66ba788f33
    f609c441bb61e78c706b807646b803714b1c4df981679e1dc79c5195b3c697fd042f0c0c78bb0deba263d3ef9a2264bd7386463fc26a014a5237ed7e51143eec
    e9d36920d2449dc8706b807646b80371a08792b1034404eb677d49eb2b9eed9f8b91ababefd8c706bafe5040957ee65200d3e0b087c7374431d019cdae70d870
    025af1404b9bbe0d706b807646b80371a08792b1034404ebdd4c62910e4aa482a984b5c814f142dfbadae1317df5ab3f23b782b3d6a37df184ed6abb421c1f02
    e359198f0d54dd04706b807646b80371a08792b1034404eb22e712c6dfe7eccad76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    5aa875be979324eb706b807646b803714faa76dd4ebef8156e56ef7b103a718f6bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331347930dd0ea548b5c0
    174aab22bc8b48c3706b807646b80371a08792b1034404ebb3a34c493507b4faaf4b7be9fedfc9a8478a87bc5b8e6cf96bf55428c35ad9f811e89b3f90b53f1c
    f55d627e5b6a5781706b807646b803710cd21e8ca845a98b0127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    f9d40bfe034dc9e4706b807646b80371a08792b1034404eba05659ea5c1551414fa6130fb0de8c9350932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    8df0563ff6b12bcb706b807646b803714faa76dd4ebef815e3c8854d9eba907f1d4e452fee093da4e033578534f961d26e9adfbcaaf6fe51c173022dc07b974d
    638ff464aec55f37706b807646b803715a6fa533133f11a3e5ed36f61e63f360c226e28d6958f7095651d10d29ebe89e9cd1b241aee3ca524f90023d786d0eaf
    f24cff2bb787655c706b807646b80371701dd54135e2845d7c63738b614a4dc1d0b01a738ef93a9d303d7240d8c3139de033578534f961d21e23b55ace376035
    fb084946fa1d2f48706b807646b803715671e59bd39a227305d2793e5127767ae07746d3d0076eb200d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    e11f20ad36e7e098706b807646b80371eeab2e0253cc6f8753823fed859af48366eaeb9fc4cc8ae15bcb4f3deed2fe5882b5425599ed1844b97ac6965124046b
    ebf1591b7680bc626bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331342b8faa1fa650af416a9a8a27fd2d97fa31bed7b19595e6545cc6ca479f16c6b6
    5b163e195ceeae4a706b807646b803715671e59bd39a22730b45656f6126dbeaae8ece02dda0bcfd60877ff0912fae9e6598c49887b4fc2b07012a1a8f02beee
    da32fce65bd9e4ea706b807646b80371bd8ecf3ecfc8ef6714361fb5d99f43506bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331347930dd0ea548b5c0
    4cda0bfb3e7f17e6f60b46ee8e8166be448af6bd68b1383883f4586e2fcc0a634e237b59546ef6f22962ea8ee267008d644126c9831a96bda118e546bf58ab2c
    064c7d10b22fd68aec4b5a01552036e1303f53704e2595d18fe1aec0698a9b90d3b99b01fef3c64498c453163ff10bcfe4b2500fe4e809c5769ab468c6f113f9
    70c9126bd9ff8882e9aa8206dccedec85651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    c930ee9bd4ca2400e26ef9f44a7eb3b5ca023470191575ccfc301e5086eb985396b3eacb99bc6a95a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    064c7d10b22fd68a472daf882b741cd8fd9475d1df4fab6d2ff3983901ebdf1bfaca85d0862a74fb0c76c4db3c95135f9dd5ccfa588ebff3bb6b2bcf56be112b
    ad70a4fb8ff671b66bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331342b8faa1fa650af416a9a8a27fd2d97fa31bed7b19595e6545cc6ca479f16c6b6
    32cd76a2a36328a92532381493787cb8d6600d5af11a4d3eb1840a4bfbabe1c93f013fb7ee415b211b4ad6a9271e801ed4155cda969bd8d9fb1b1de5b0925d59
    46ca60d9e0a03ec1cfe1d30080fa8985e3570c3308686a4dbe7209490363213f45e4e160e3aa04d7a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    9eaf82adc2a1140d34c73dcbf92dd8729c4005bcd9ca79e6e00eefbd63f1d45d8492e52ca99071373360b3b2bcd4874aef23bbe4f31b58a8673b81ca19be4e33
    8e12dea80c549de261698f310be5a400f78f01ca7cd3184ca95fd1712bcaf1b029b48a33a73df9caaf399d32d282acb6a263d3ef9a2264bd73ac5403918b2efd
    928d7a9f462cf2ed706b807646b8037150eb858f9032cc838b0547476f2f18a15d4b44c85b70670f7e695e5d531063625a4c9a26c2a42486b77986be7141a48f
    1b6bebc0bc33482c706b807646b80371bd8ecf3ecfc8ef6745b5a70a5cc0245b5651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802e323c1799b4666e62
    07c82d144c68cf87cd9f9b0fe66d8ad11aedfeffe85ebe258d915cdb7782fd416598c49887b4fc2b7857de061e2a26efa85bfcd7236670cdeb605ebf76f26de2
    1632a67cf5c03a1a706b807646b803717c63738b614a4dc1deb29c76e244f6ee66eaeb9fc4cc8ae15bcb4f3deed2fe58f20766bdac48276ea80c2743bc5ec9e0
    f0acca179947ec8f6dba65afb526cbc1a263d3ef9a2264bd7386463fc26a014adcae02a052f89a2da290117246b6bdc47e283b747a56c79421cde62a0a842d2d
    f57b0f2f4f3d276e706b807646b80371eeab2e0253cc6f8774a1258979547e3db7e56e956fec2f26ef1d7357d3c4e2f3644126c9831a96bda118e546bf58ab2c
    593e80cc430081d2706b807646b803710b45656f6126dbea8ba75e1a7d67df4598edc312c449029b94ef342977743ad062d766f77596a54b1c022559c34d47a8
    d6aca196616365d3706b807646b80371eeab2e0253cc6f877ffffa9baf890d4866eaeb9fc4cc8ae11b9fb80fc79e7cd8b529248e59261b2c62b84e5bac7fe806
    290ad72d9c5d86d6d5ba6b0a204ed1235651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    9209d3ab4a447b3e0529bb43a7ec9944cbc940513e636f1e7a8ee61b2ac7ee7875398a5ed1f1b9156bf55428c35ad9f818b1e200d5b367e949f39e38b6c0fccc
    bdd8d6b45d26c9f3706b807646b80371143f62011610c8e26de7d7947cf2bfa76bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331347930dd0ea548b5c0
    b965afc66411a939706b807646b80371fe2486f8cdb753dd8fa9d028134572658df8cf962e0b71f650932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    064c7d10b22fd68ad6451f700dbd4eeafd9475d1df4fab6d5829074c65631300d3b99b01fef3c6449b399e078b2806b680890c5e795f5da7f08aa6603ffcf1aa
    a8835ce432d01b0c1db9be5844c9b7c84ec5850e704dd631fbd67efb1043a1e26efcae405adba980ca47c4a8e8c8d49f752925d49cb16d497a3fbd26708b2a8e
    32cd76a2a36328a92532381493787cb8c7c0ff6aff14e47c073d57a0eaa16b2e60c9783cd34f18105960294be34dfb0c61698f310be5a400c99cc804ae839bdf
    fd6bb2445a39ab416598c49887b4fc2b7857de061e2a26efa85bfcd7236670cd3e51762787380085b0f5c467238a30432f65f2e99cc333ed7cdf306a4c574167
    71011f181f54b3e361ad8839db814189a8d6984e08c7aad08bf4f6f2e78aa0a8b9b3abf75e62eaab52e00aa790b455bb3c185b56871dcecb3b300708695416e3
    a7016332727eeac3706b807646b80371eeab2e0253cc6f876d84478bc105beae23ae7ba6d36cc4bd50932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    9f337bb24085865c706b807646b803710b45656f6126dbea2c26e93bf2541112a43dc3d884d87a691962f61c1a635c8d62d766f77596a54b1c022559c34d47a8
    80b5fda8ff9d3f4e706b807646b80371fe2486f8cdb753dd857295c9975dd8465f1937206921a2ed640b08cecbb6cffe042f0c0c78bb0deb673b81ca19be4e33
    064c7d10b22fd68a7509c136893a3e2e303f53704e2595d1e5e7fade4086c0d1d3b99b01fef3c64498c453163ff10bcfe4b2500fe4e809c5769ab468c6f113f9
    70c9126bd9ff8882e9aa8206dccedec85651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    c930ee9bd4ca2400e26ef9f44a7eb3b5ca023470191575ccfc301e5086eb985396b3eacb99bc6a95a48e116be34e416db5f1c17ee7956303ed52cc602f48c27b
    88070a17816250e7706b807646b803710b45656f6126dbead22a2727f10326dfd76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    25dadebd820afd72706b807646b80371989d190a69797eee0127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    76c226c74162658e706b807646b803710b45656f6126dbeae398f727c47c7615b41429200bc9d6b4cb05648a7343990262d766f77596a54b1c022559c34d47a8
    090e4b6528d980ae706b807646b8037115deb1a5e6728cf5143f62011610c8e2f2fd3f0f55709a15303d7240d8c3139de033578534f961d21e23b55ace376035
    9eaf82adc2a1140daf62c7e801e29edb9c4005bcd9ca79e65e53eb09280546c98492e52ca990713774bd84a1f90ee88c146628815e2daa418b8f92ada6ab6779
    88f02d15ca9c6f41e73070a45f1d549c6598c49887b4fc2b7857de061e2a26efa85bfcd7236670cd3e51762787380085b0f5c467238a30436445e6c14ba2c5fa
    58cf452d198b3802706b807646b803713ccc9fb8d5c7e25e7c63738b614a4dc13a12794a0bbb04c2303d7240d8c3139de033578534f961d21e23b55ace376035
    709cd66b96967eeb706b807646b803710b45656f6126dbeada88a3aa1e8e53f6d76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    8818260e40cfae59706b807646b803712549b74dc22585560127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    afb57ee19c9d50ea706b807646b80371143f62011610c8e2ae1e8de5e31346c1805f3dc1f93d56fe7e695e5d53106362e085717002817eb3117c43488ffc6d6b
    76777896a7ce37a2706b807646b80371debee9ea7afb849e0127ad895999246523b782b3d6a37df11db9be5844c9b7c84ec5850e704dd631cbf1cf296810270b
    3d875a9a87f9d624706b807646b803710b45656f6126dbeaf6250f7e15a5c10cd76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    9eaf82adc2a1140d976633e3a662b0a89c4005bcd9ca79e6894381d170438d328492e52ca990713774bd84a1f90ee88c5250164eead6fad4133faeaa1ac7e1ab
    55136b92d0559ec4e71f71e1875841714cc7d4f7427922f33dbf35e2592bf3d7e6cc5e557a3c106367e851ead15b2a91de6ccc763475b3ceb88a6c9366dff5dc
    8e641f8c2424c2e1706b807646b80371a97b765744e54e1826d0fbb139962a0b478a87bc5b8e6cf96bf55428c35ad9f818b1e200d5b367e949f39e38b6c0fccc
    9eaf82adc2a1140dcd9f9b0fe66d8ad1e3b798de2a9b9eecaa2f1d7584e4b8d2ce5ec34e6f8ad1ca09a503e1af40f07a6933223ff0a8eca47cf023c2239db233
    7c6a057502825b8b6bf55428c35ad9f818b1e200d5b367e934cb1f5e9a6331342b8faa1fa650af416a9a8a27fd2d97fa31bed7b19595e6545cc6ca479f16c6b6
    40f41cdf5245bcc08f8d74c047af5be8387e82ba91c98af427876424abadc0a7280a3d8e4636feaa53456d9034a59a02e827ca08aceff3d79c7a4bc0de56f663
    9eaf82adc2a1140d5bd1d958b85c63379c4005bcd9ca79e6d58cdad0fec876c48492e52ca990713774bd84a1f90ee88c5dba07e1efa84051940d46f618ddb284
    a63f11eaaca09401b5f1c17ee7956303e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956af92be55228ec5c32
    3f2d39c3473bdd81706b807646b803710b45656f6126dbeaa7ac554b70945d8dc82ab3b2f8f47edb53a4999cf475b1ba62d766f77596a54b1c022559c34d47a8
    064c7d10b22fd68a0fb9a87d5a97a04b3d59dfa5c6e6246c6342ce344f4132ecfaca85d0862a74fb5589c49a9624f695cda4baa068a73fff6f6620a49d5db2bb
    ca7f88d3b0d2438ab5f1c17ee7956303e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956af92be55228ec5c32
    80409ca1121b04d7706b807646b803713ccc9fb8d5c7e25e74dc3a64e1e990ed478a87bc5b8e6cf96bf55428c35ad9f818b1e200d5b367e949f39e38b6c0fccc
    92491360359d2ac4706b807646b803717c63738b614a4dc1ede42e8a91db457b66eaeb9fc4cc8ae15bcb4f3deed2fe584430a7a5b441e4d3a80c2743bc5ec9e0
    5f1937206921a2ed7856c6afe220f6455651d10d29ebe89e9cd1b241aee3ca527d25d62c4583802eb516c6374f716458cdc98df979ee8e018818cbd4210f0def
    430882ca1e45ea8b706b807646b803710b45656f6126dbeaffb1728fb299b3c25c702c3de286e0aac1cb60b9845d858e24fdfd9bb2e10b0766f5d7227ff3c671
    a155848e3bbce6f3706b807646b803710b45656f6126dbea54054943b5fb4f1ad76167baccb438ba00d3e0b087c7374442cdae931a3d3892436d2b66847f52b9
    e713cfefd199f1eb706b807646b80371fe2486f8cdb753dd2b0e7197a01f581383a1af2b064b63d950932f91c29cb99b710f626c2faf14a6ed52cc602f48c27b
    2b3f0796f933b05af60b46ee8e8166bed102992399a397df1ede05ad024319068bcc8a7f6eba11314e3b5b908c2815ff5651d10d29ebe89e70605af949aa2245
    9eaf82adc2a1140d752f7113017609339c4005bcd9ca79e6026a90a9bc342ef78492e52ca990713774bd84a1f90ee88cf2bc79891bc1c93fd9997f6750464469
    a63f11eaaca09401b5f1c17ee7956303e033578534f961d26e9adfbcaaf6fe5125d7a787f2d39803f23a97ef1f1d051abcf4b0ff0007956af92be55228ec5c32
    e07dfe0d2e28b89c706b807646b803710b45656f6126dbea58e99fd91daf668a81def0c67df4b206955f478f324f6d7f24fdfd9bb2e10b0766f5d7227ff3c671
    09a7c1f8b05a8ac1706b807646b803717c63738b614a4dc11bfbffa661b63638691018eed3b49c3685d8806da1e0ac981625a916457b09524c721f1915d81d71
    d177348d2deab5c2706b807646b803715671e59bd39a2273715ee7be0cf2a78ffaeaa281e22d723e644126c9831a96bd0913a741f2f1d533dcfb55a634b33adb
    60c9783cd34f1810706b807646b80371e5494a25d92d58bfaad0cae5ebf3019a0913a741f2f1d533c167b19f5561b8d10a3dca7c9f0c7a1a07ca2e46d08f789f
    9af710ac7afcd4a8706b807646b803716d2b3ea68bf556be6f351d1b39770686478a87bc5b8e6cf9691018eed3b49c3685d8806da1e0ac982c66f1c690743c90
    fab9cf2b7c040381706b807646b8037150eb858f9032cc830277ed7ba7f99963691018eed3b49c3685d8806da1e0ac981625a916457b09524c721f1915d81d71
    be52e6aa176ef44b706b807646b8037115deb1a5e6728cf50b95d65fc212ad34478a87bc5b8e6cf9691018eed3b49c3685d8806da1e0ac982c66f1c690743c90
    b29471f7f94cc38f706b807646b80371b10f4f7d78547f3a0127ad895999246523b782b3d6a37df130cb792a729d977e348481f601fee253f54692846f76b1c0
    0b22eb7d0b342b1c706b807646b8037115deb1a5e6728cf5eb7d47e44bd5ce9f478a87bc5b8e6cf9691018eed3b49c3685d8806da1e0ac982c66f1c690743c90
    3e761c6835cdd8d5706b807646b803717c63738b614a4dc15906b005a38828e7691018eed3b49c3685d8806da1e0ac981625a916457b09524c721f1915d81d71
    7d39dd9f81bbcdfd706b807646b803715671e59bd39a22731c90425132b9714749bcb2e9b7241eb4644126c9831a96bd0913a741f2f1d533dcfb55a634b33adb
    f850674c77dc0a72706b807646b80371701dd54135e2845db5a5d7fe347b969f478a87bc5b8e6cf9691018eed3b49c3685d8806da1e0ac982c66f1c690743c90
    93d3808648446fd7a60fd3951de4fe94b6c36883137f300162d766f77596a54b693b06cb62c8947be6b9412e4bab9f0a8218fbb9c051aaeb0d4817371b05d633
    $CDNENCFINISH
    .ENDS UCC25600_TRANS

  • Hi Ardeshir,

    The UCC25600 spice model looks this way because it is an encrypted model.

    Check how much current is getting pulled out of the RT pin. If too much current is pulled out of the pin, the controller will not switch. 

    Best Regards,

    Ben Lough

  • Yes, the current out of RT pin is close to 10mA (higher than what specified on the spec sheet)

    Is it related to soft start pin? For now I'm just applying 5Vdc to SS pin.

    btw, I have done open loop simulation with pulse generators and things work as expected. Just need to make the controller work properly.

    Thank you,

    Ardy

  • Hi Ardeshir,

    Try disconnecting the opto-coupler for now. Perhaps something is not quite right there. See if RT pin becomes something more reasonable when R10 is removed.

    Best Regards,

    Ben Lough

  • I did three experiments to see if controller works:

    1. completely disabled feedback circuit and instead added a current source of 3.5mA to make controller to pulse at fixed frequency and open loop.

    The GD1 and GD2 are still not producing PWM but there is a output voltage (in green) for few microsecond.

    2. I removed the entire FB circuit and added a 3.3V DC supply to R10 and removed the DC supply on SS pin:

    Still no PWM; but, RT current dropped to 1.5mA.

    3. If I remove R10 and the optocoupler, the RT current is even higher -12mA

  • Hi Ardeshir,

    Sorry, I don't think your images made it into your post. Could you try posting them again?

    Best Regards,

    Ben Lough

  • Hi Ardeshir,

    As a side comment, it does appear the PNPs are upside down in the totem pole drive structures. I would suggest to flip them to get the right connections.

    Best Regards,

    Ben Lough

  • Sorry - I noticed it doesn't uploaded images - here are the images for each trial:

    I did three experiments to see if controller works:

    1. completely disabled feedback circuit and instead added a current source of 3.5mA to make controller to pulse at fixed frequency and open loop.

    The GD1 and GD2 are still not producing PWM but there is a output voltage (in green) for few microsecond.

    2. I removed the entire FB circuit and added a 3.3V DC supply to R10 and removed the DC supply on SS pin:

    I did three experiments to see if controller works:

    3. If I remove R10 and the optocoupler, the RT current is even higher -12mA

  • Hi Ben,

    I forgot to mention that I have already simulated the same schematic on TINA TI with no problem and I am able to get desired output with ZVS.

    This is why I thought maybe something is wrong with the PSpice model. 

    Please see images below:

     

    What other resonant controller do you recommend from TI? I have looked at  UCC256303; but, there is no PSpice model available.

    Regards,

    Ardy

  • Hi Ben,

    I was able to make the controller functional - I made changes to RT1 and RT2 resistors and removed the BJTs and the controller now works. I initially used the BJT per reference design in the datasheet. Can you please explain why it's necessary to have BJTs as part of gate drive circuit?

    Would you please provide LM293AD spice model? from the website, it doesn't appear that the file I downloaded is a .lib or .olb file.

    Regards,

    Ardy

  • Hi Ardeshir,

    The BJT structure is just a totem pole gate driver. it increases the current driving capability of the gate signals going to the gate drive transformer. The totem pole driver is not explicitly needed. You may also pair UCC25600 to a half bridge driver such as UCC27714. You can refer to PMP20694 as a reference.

    Best Regards,

    Ben Lough