This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD95496QVM: Voltage range for the TAO (Temperature Amplifier Output) pin

Part Number: CSD95496QVM

Hello, I have a question about the TAO (Temperature Amplifier Output) pin. According to the datasheet, the max voltage for this pin can be VDD+0.3V (5.3V).

In my design, the TAO (Temperature Amplifier Output)  is fed to an ADC input which is limited to 3.0V. So I am a little concerned that the voltage level is too high for the ADC input. 

Thanks.