Hello guys,
I am using LMZ14202H as a BUC Regulator in my application.
1. Input 42V to generate 28V @ 1A - This has power dissipation of 1.8W
2. Input 42V to generate 5V @ 1.2A - This has power dissipation of 1.3W.
My query is
1. Can the package handle this Power dissipation
2. What is the maximum power dissipation that the package can handle.
I am using a FR4 0.8 mm/1oz PCB.
What are the extra precautions I need to take care in schematic and Layout.
Thanks
Narendra