Hi,
Please can you confirm: What will be the state of SO output pin in case of loss of power? Will it be FLOATING or are there any internal circuits / pull devices that will pull the output to GND?
My assumption is that this is a push-pull output with no internal pull circuits so that in case of loss of power, nether high-side nor low-side of the push-pull stage can be switched on, so therefore the output pin will be FLOATING - is this correct?
Also, from other answered forum posts, it seems that NONE of the input pins (G / SRCK / RCK / CLR / SER IN) have any internal Pull-up or pull-down devices - is this correct for ALL inputs?
Therefore if two devices are daisy-chained with no external pull-up/down devices connected, and the first one loses power, then the serial data output line from the first one (serial input to the second) will be FLOATING? - is this correct?
Thank you