This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5155: Low efficiency compared to theory calculation

Part Number: LM5155


Dears,

My customer used LM5155 for boost -- input 7.2V, output 24. Below is circuit and layout. Customer actual test efficiency is only 85%, big gap compared to theory calculation as high as 95%.Please help check.

  • Hi Garrick,

    efficiency is impacted by a lot of factors (inductor, switching frequency, FET, diode, output current, input voltage ...). 

    Do you have a BOM list to look at? 

    And what is the output current?

    At low input voltage and high output current the efficiency is expected to drop to a certain extent (see Figure 10-2 in the datasheet).

    Also, could you please let me know, what is the theory calculation based on?

    regards,

    Julian

  • Hi Julian,

    Added customer test below. Will check the BOM.

    1, Output 1.5A(23.57V), and input power 41.544W(7.2V*5.77A), so eff. = 85.1%

    2, Output 0.1A(23.77V), and input power 2.715W(7.2V*0.377A), so eff. = 87.6%.

    From the test above, it seems light load(0.1A) efficiency is little higher than heavy load(1.5A), which is different to spec.

    BTW, the theory calculation tool is LM5155 Boost Controller Quick Start Calculator