This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
Psl kindly help for below questions, thanks.
1. Pls help review schematic as below.
if TPS26600 work when TP68 provide 5V?
2. If SHDN(pin 7) have voltage(Avdd Internal pull high) ?
Thanks, Ian.
Hi Ivan,
Please remove R120 to make TPS26600 work at 5V.
SHDN has internal pull-up, you can leave it float to enable the device when Vin is applied.
Thanks and Regards, Rakesh