This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36506-Q1: Output Voltage and Efficiency

Part Number: LMR36506-Q1

Hello,

I am looking at the LMR36506-Q1 for an application targeting an output voltage of 24 V at 0.5 A max.  I've attached the Webench design here: 

https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=4F9012D9EE5EDAFD 

I do have a few questions here.  Is this device capable of a 24 V output?  I believe so but I wanted to confirm as well since I couldn't find a specific range in the datasheet.  Also, there was a strange efficiency waveform on the Webench design attached below.  Is there a reason for this valley at 0.2 A on the efficiency curve?