Hi,
My design spec. is
TI Part : LM5175
Vin range : 8V - 27V
Vout = 24V / 6Amax
I am facing problems with output regulation in buck-boost and boost mode
#1. At Vin = 24V, Vout is 24V with light load
#2. At Vin = 24V, Vout is not regulating to 24V 1A load (Refer. Fig 1)
#3. As Vin reduces from 24V and with light load, Vout is not reaching 24V (Refer Fig 2)
#3. The SS pin shows a sawtooth waveform when Vout is not regulating to 24V (Refer Fig 4)
#4. COMP pin waveform is pulse like and is not settling to a stable level. (Refer Fig. 5 and Fig 6)
I used "LM5175 Buck-Boost Quickstart Tool" for the design and the screen shot is attached. (Refer Fig 3)
Kindly help me to resolve the issue.
Thanks,
Thomas Joseph