When bq24072T supply on disconnect battery (open) condition, VBAT occur nearly 2Hz switching.
※Ch1: Vin, Ch2: VBAT
Please let me know about three points below for above operate.
①I think that the reason is affect of safety timer signal from /CHG pin, correct?
②Is there way to reduce VBAT switching on disconnect battery condition?
My idea is /CE set High, or disable safety timer (TRM to GND), I want to know the other idea and my idea correct or not.
(If possible, I want to avoid /CE: High setting by keep in mind of total system setting.)
③About battery connect and disconnect on the same condition, is below setting no problem?
・Over discharge (1.5V ~ 2.8V) to remove (0V)
・Re-connect 1.9V battery
・Connect the deep discharged battery: less than 1.5V
Best regards,
Satoshi