Hi,
Our datasheet says PG pin should pull up to VREG5, with 20K - 150K ohm resistor, is there any risk if using 4.7K resistor, pull up to 4.7V?
Thanks.
BR
Mason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mason,
I did not find a max value in the datasheet but since the sink current of 1mA (4.7V/4.7k) is even lower than the typical(5mA), it should be fine to use a 4.7kohm resistor to 4.7V.
Thanks,
Amod