Hi team,
My customer is using the TPS7A8300 in ANY-OUT mode for a 1.2V output but now need to increase output from 1.2V to 1.3V. They need to use the feedback resistors instead of ANY-OUT mode by making the following changes:
- Uninstall R450
- Install R446 with a 7.5K resistor
- Install R448 with a 12K resistor
- Uninstall R447
Question - Since they have to disconnect SNS from OUT to get out of ANY-OUT mode and use feedback resistors, can they still leave C500 installed for the Cff? I've always seen the feed forward cap from the output to the feedback pin, but datasheet is recommending the Cff be between SNS and FB instead of OUT and FB. Cff being between SNS and FB in ANY-OUT mode is essentially the same as having Cff between OUT and FB since SNS has to connect to OUT anyways.
Connie