Hi,
I am working on reference design for TPS54327, I am using the following values from WEBENCH designer:
Vin : 12 V, Vout=5V, L=5.6uH C=1000uF, CSS=10nF
The converter working as expected on no-load condition but as soon as I load the converter ever slightly (47 Ohms), the output voltage drops to 100mV.
Update: Seems to be working for Input Voltage around 6.5V and is giving regulated 5V as output, But if we increase the input voltage beyond 6.5V, It is not giving the output as few mVs.
Can someone help me fix this?
Thanks,
Prem.