Hi TI Engineers,
May I know what causes the output of the LM76005 switching regulator to oscillate between 1V to 2V when the output is set to be at 5V and the input voltage is set in the range of (24V to 31V)? At lower input voltages (~5.5V to 10V), it was able to produce the 5V output voltage but it was a 5V sawtooth output instead of a straight 5V output.
Best regards,
Wei Jie Ng.