This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My board includes the following components:
1. Xilinx Spartan 3E FPGA: 3.3V, 2.5V and 1.2V
2. DDR SDRAM: 2.5V and 1.25V
3. OPA3693: +5V and -5V
4. TVP7002: 3.3V and 1.9V
5. LCD backlight LED driver: six serial connected LEDs (each LED requires 20mA current and 3.2V voltage)
Any input voltage range will be ok.
Thanks.
Have you tried TI's processor attach reference designs in the TI Power Management section?
Hai,
There are numerous reference designs for your FPGA here: http://focus.ti.com/analog/docs/refdesignovw.tsp?familyId=64&contentType=2&genContentId=34823
Please pick one that you want to use and then we can work on getting the other voltages based on what the reference design already provides.