This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
We are using TPS61241YFFR for our design and there is a phenomena occurring which increases the voltage beyond 5 V. I am assuming the cause is the inductor at the input but want to be sure.
In the graph below, the div is 1 V and the orange one is 5 V.
The schematic is below,
Can we also use TPS61240 for the design instead? The difference seems to be only in the valley current and the maximum output we need is 4.5 mA which is below the difference between 40 and 41.
Regards,
Hi Matt,
Thank you for reaching out.
I can't the waveform very clearly. What's the time scale? Is this waveform captured by digital oscilloscope?
Can you also share the layout on E2E for us to further check?