This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51561H-Q1: Boost Converter

Part Number: LM51561H-Q1
Other Parts Discussed in Thread: LM5156, LM51561

Hi all,

I would like  to develop an Boost converter using LM51561H-Q1.

The input voltage is 24V, the output voltage is up to 150V @5A .

Are these specifications compatible with the IC.? On the datasheet I read  a wide input voltage up to 65V. The output voltage on TI workbench is up to 150V.  What advice could you give me? If these specifications don't meet the IC requirements may you tell me the properly IC?

Thank you so much

Manuel